How to pick a specific point for Smart Measure?

Creator
Creator

How do you pick a specific point, e.g.. a center point, intersection or end point, using Smart Measure if the software doesn't automatically pick the point? Are there keys you can press, like C for center to select the point you want to measure from or to?

6 REPLIES

Re: How to pick a specific point for Smart Measure?

Esteemed Contributor
Esteemed Contributor

The measure command has an option on the Command Bar to set the keypoint filter preference.  If you cannot select a keypoint it is probably due to the filter restricting it or if in an assembly, the part you are trying to select on is inactive.  Smart Measure's filter is at the right of the Command Bar...

measure.png


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: How to pick a specific point for Smart Measure?

Creator
Creator

Thank you for the reply. I am running the ST5 version of the free 2D Solid edge and this does not appear to be in there?

Re: How to pick a specific point for Smart Measure?

Esteemed Contributor
Esteemed Contributor

Hi there,

 

You'll need to use the "Distance Between" dimensioning tool to get the options you're looking for....make sure all of the "IntelliSketch" options are checked on.

 

SE_ST6_Draft_IntelliSketch.png

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

Re: How to pick a specific point for Smart Measure?

Creator
Creator

Thanks for the help.

Re: How to pick a specific point for Smart Measure?

Esteemed Contributor
Esteemed Contributor

I was assuming the 3D environment because it was not specified...  You are right, the Smart Measure command in Draft does not have the keypoint filters, as per it's explanation, it only measure elements or angles between elements.  If you want to measure between keypoints, you need to use the Measure Distance command which will access keypoints based on the Intellisketch settings... Or use the regular Dimension commands as Sean stated if you want them to persist.


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3

Re: How to pick a specific point for Smart Measure?

Legend
Legend
One trick with smart measure is that it will only pick an endpoint or center point on the first pick but it will act like Measure Distance on the second point and allow you to pick midpoints and so forth.
Using SE since V12, 2002