Cancel
Showing results for 
Search instead for 
Did you mean: 

How to resize connector dot/circle?

Experimenter
Experimenter

I am creating a bot wiring diagram in mm and i am not finding an optio to reize the dot/circle/arrow for connectors. The current size seems to be 1mm.

1 REPLY 1

Re: How to resize connector dot/circle?

Valued Contributor
Valued Contributor

Hi Greg

You need to create a new style( preferred ) or modify the existing style.

Go to view styles

Dimension and the style currently in use

select modify

then "terminator and symbol" tab sheet

adjust "measure size"

then apply.

This will change the dot size for all dots using that style. This can be a pain so I recommend creating a new style and setting the size dot you require. Then apply that style via the option on the command ribbon for only the dots/connectors you wish

 

Pete