Cancel
Showing results for 
Search instead for 
Did you mean: 

How to save as DXF

Pioneer
Pioneer

Hi

I have just finished a CAD model/part  and I need to send it to the manufacturers/prototype company, they are asking for a vector format, DXF. How do I save my design as a DXF as I can't seem to find it on the save selection. Or what other format available from solid edge will work instead of dxf?

Thanks

Kind regards

Ravi

13 REPLIES

Re: How to save as DXF

Legend
Legend

Make a new draft file and import your model at 1:1 scale on the view you want then save the file as a dxf.

 

Yea I don't like it either...

Re: How to save as DXF

Gears Phenom Gears Phenom
Gears Phenom

They're not asking for a 3D wireframe dxf are they?  

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1

Re: How to save as DXF

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Good question Kyle. I was thinking the same since Ravi's post mentions DXF from a CAD model/part

 

~Tushar

Re: How to save as DXF

Pioneer
Pioneer

Thanks guys,

Just uploaded them on the draft and saved them as dxf.

 

Re: How to save as DXF

SE should really let you create a DXF from the 3D model without having to go into draft mode.  SW will let you do this easily and then you just specifiy which views you want it show in the DXF.  Then you specifify if you want them as seperate files or separate tabs.

Owner: Scott Lester Drafting & Design
Designer: Rotork Instuments

Re: How to save as DXF

Legend
Legend
The ability to generate DXF of the individual parts of an assembly would be awesome. Our valves are mostly plate fabricated with anywhere from 6 to 50 individual parts that must be individually turned into DXF files for the nesting program. It can be a chore to say the least and always a fear that we missed something.

Re: How to save as DXF

Valued Contributor
Valued Contributor

hi,

I have th same problem, only that when I try to save the file in the draft area as DXF. it says that there is a file translator Error. what do ido??

Re: How to save as DXF

Legend
Legend

I have a macro that will create my .psm DXF file with just a push of a button, no draft necessary.

 

One of the guru's on here had a macro to give total cut length of a .psm file, and part of that macro can create the DXF at the same time, putting it in the same folder as the source .psm.

 

Here's the discussion that brought about the macro solution:

 

http://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/display-total-cut-length-for-manufac...

 

ST8 MP9
Go FAST, or go home.

Re: How to save as DXF

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Solid Edge can save dxf from 3D model, but you have to be in sheetmetal environment and use Save as Flat pattern command. Maybe this is not an elegant solution but works! Smiley Wink

 

Here is a short video:

 

BR,

Imics
http://solidedgest.wordpress.com/