How to set a specific view config and rotation style when loading or following load

Experimenter
Experimenter

Hi Folks --

 

I have a situation where I'm loading a ton of parts (STEP files) into solid edge for nice, stylized images of them.  An example is below.  What I would like to do is either be able to have a macro that rotates the parts automatically (X:45 deg, Y:45 deg) and sets the view options to reflect this orientation and display mode...Or I would like to have a script or push button customization that can do this.  The alternative is that I have several hundred (possibly 1000+) parts that I need to painstakingly open and rotate and change their view options for.  

 

Does anyone have suggestions on where to start?  Is there a scripting language that I can run inside of the ST6 or do I need to build compiled add-ons?  Is there a command line tool that lets me do this invoking SE from the command line, passing it a file name and some commands, and having it do this automatically?

 

Any help you can provide would be awesome!!!

 

Image to follow.

 

Best regards,

 

Matt

 

 

3 REPLIES

Re: How to set a specific view config and rotation style when loading or following load

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
Why not simply take isometric views?
Mark

Re: How to set a specific view config and rotation style when loading or following load

Experimenter
Experimenter

That's possible but none are the ideal angles and too much finagling for the 1000+ parts I've got to do.  Is there a way to create this view and then apply it to each file that I load?  Otherwise it's a lot of manual effort for something I would expect to be able to just hit a button and have applied.  Best if it could be scripted. Any suggestions would be super helpful!

 

Many thanks,

matt

Re: How to set a specific view config and rotation style when loading or following load

KennyG 2nd Gear
2nd Gear

You need to use Visual Studio's VB or C or similar if you would like to automate SE.  You can even use VBA in Excel but since Visual Studio Express is free and it gives you more options, I would recommend it.



Ken

Production: ST10 MP3
Testing: SE 2019