Cancel
Showing results for 
Search instead for 
Did you mean: 

How to stop dimensions being so intrusive?

Experimenter
Experimenter
Spoiler
Dimensions invasive.jpg

As you can see I have Protrusion 2 selected which represents two small LEDs. Each dimension within its sketch seems to be about 20 times the size of the actual feature, obscuring my vision of the part and meaning I have to right click and select other every time I want to select a face.

 

It seems to me that it isn't registering the size of the feature, only some overall base preset for the dimensions. If I were to add a 100x100mm solid next to this one, I doubt I would have any issues with intrusive dimensions. Is there a way to get them to scale based on the sizes I'm working with or how zoomed in I am? This is really causing me some hassle. Thanks.

2 REPLIES 2

Re: How to stop dimensions being so intrusive?

Phenom
Phenom

Hello,

 

Try doing the following:

 

During skeching you have to click on: PMI as pixel size.

And you could resize your dimensions with the small A unter the: PMI as pixel size

 

 

Yasser

 

dimension_PMI__Pixels.jpg

Re: How to stop dimensions being so intrusive?

Experimenter
Experimenter
Perfect, thanks for the help