Cancel
Showing results for 
Search instead for 
Did you mean: 

How to use piping & fitting parts which is downloaded from standard partslibrary

Experimenter
Experimenter

Hi, i need a help in using downloaded piping standard parts in xpress route.

Steps followed: opened solid edge assembly > opened standard parts library > selected required pipe / fitting > open > saved in a folder.

In xpress route when i try to browse the saved pipe as cross section it is not accepting and showing error. 

 

But for pipes when we change the variable property from "d" to "Diameter_1" then it was accepted as cross section in xpress route.

 

same time i'm not able to use any flange in express route. 

 

please help me to solve this issue. 

1 REPLY

Betreff: How to use piping & fitting parts which is downloaded from standard partslibrary

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Mahesh_S

 

 

first of all the basic question: "Do You have licensed the Piping library too?"

This is a basic requirement besides xPresRoute license to use those library too.

 

And if Yes, then have to selected the correct class of pipes to be used together with that pipe/fiiting/etc.

 



regards
Wolfgang