Cancel
Showing results for 
Search instead for 
Did you mean: 

I can't open a 2D Autocad.dwg in Solid Edge

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

When I try to open the 2D file from Autocad, Solid Edge give me a message " The translator fails when the selected Autocad file was opening". I tried to change the SEACAD.INI for another one from a laptop that works correctly, but I have the same problem again. I have also checked that the configuration and the place of seacad was the correct one.

 I have ST10 and the MP5 of Solid Edge. 

 

Thank you

5 REPLIES

Re: I can't open a 2D Autocad.dwg in Solid Edge

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Can you attach the DWG for checking ?

I believe no setting in the INI file should result in failure to translate.

Does the other laptop have same SE version and MP version ?

Re: I can't open a 2D Autocad.dwg in Solid Edge

Gears Phenom Gears Phenom
Gears Phenom

I think the .ini is for export, not for import.

...........................................................................................................
Solid Edge 2019 & AutoCAD 2019 user

Re: I can't open a 2D Autocad.dwg in Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Joris, Pretty sure it's for both. Else why would there be an options dialog for both?

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: I can't open a 2D Autocad.dwg in Solid Edge

Phenom
Phenom

Hi @Dperezjorge

 

What I suggest is to use Draftsight Free to open the DWG file, and re-save it.

 

regards,

 

Arek

Re: I can't open a 2D Autocad.dwg in Solid Edge

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

We have had a few issues with the translator failing due to a corrupt SEACAD.INI file.  To fix, we set it to the delivered SEACAD.INI in C:\Program Files\Solid Edge ST10\Preferences\Translators folder, then make our Option changes and save it over whatever we had previously been using.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com