Cancel
Showing results for 
Search instead for 
Did you mean: 

I can't use UNDO at the family of assembly.

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

The UNDO button is grey, so I can't use it at the  Family of Assembly. Does anyone know, why? Does anyone have a logical explanation?

6 REPLIES 6

Re: I can't use UNDO at the family of assembly.

Gears Phenom Gears Phenom
Gears Phenom

I'm taking a guess here...  have not tested or verified myself...

 

BUT...  check to assure that "apply edits to all members"  is checked on... 

Matt Johnson
Solid Edge Certified Professional
Solid Edge 2019 (SEEC) - Production
NX12 (Tc Integration)
Teamcenter 10.1.7
Highlighted

Re: I can't use UNDO at the family of assembly.

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter
Matt,

It does not help to solve the problem. Smiley Sad
I activated this when I created the Family of Assembly.

Re: I can't use UNDO at the family of assembly.

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I filed an IR for exactly this (in an alternate positions asm)

 

This asm had the Undo button disabled, didn't know why.

Then I noticed it was an Alternate Positions assembly. To rule that out I did some checks.

 

Populate a member > member has Undo enabled

Convert back to Alternate Positions > Undo disabled.

 

PR 9491792 

Re: I can't use UNDO at the family of assembly.

Siemens Phenom Siemens Phenom
Siemens Phenom

I do not see why this was logged as a PR – it explicitly states in the Solid Edge help that Undo is *not*supported in Alternate Assemblies:

 

http://docs.plm.automation.siemens.com/tdoc/se/2019/se_help#uid:xid1129777:xid1323753:index_assemble...

 

2019-05-24 15_45_49-Siemens Documentation_ Alternate assemblies impact on Solid Edge functionality.png

Re: I can't use UNDO at the family of assembly.

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi Dave,

Thanks for clearing that up, I didn't know about the Undo-restriction.

 

PR'ing the IR however was a GTAC decision after uploading the files. I think GTAC missed the fact that it was an Alternate ASM. I believe the PR is still open.

Re: I can't use UNDO at the family of assembly.

Siemens Phenom Siemens Phenom
Siemens Phenom

Oh trust me, I realise that if this is a PR it made it through GTAC :-(


As to the status of your PR, already closed, unsurprisingly, as "working as designed" :-)