Cancel
Showing results for 
Search instead for 
Did you mean: 

I closed the "part library tab" in ANSI Assembly, how do I get it back?

Experimenter
Experimenter

I closed the "Part Library Tab" in ANSI Assembly, how do I get it back?  I tried closing Solid Edge and reopening a new ANSI Assembly and it is still gone.  I spent hours trying to figure this out, but I have had no luck.  Any help is geatly appreciated.

4 REPLIES 4

Go to the View tab, and on the far left side of the ribbo...

Phenom
Phenom

Go to the View tab, and on the far left side of the ribbon bar, there will be a group called "Show". Click on the top Icon, and a dropdown list will appear that allows you to turn on and off all of the different bars to display on the left side of the screen. When a toolbar is open, click on the thumbtack in the upper right corner of the toolbar to pin/unpin it to the left side of the screen.

-Dylan Gondyke

Re: Go to the View tab, and on the far left side of the ribbo...

Experimenter
Experimenter

I have the same quastion - I can't see teamcenter feature library on my screen (lost it somewhere). But for another hand when I go to View - Show - Pan - Teamcenter feature library I see that it's turning on.

How I can see it or return to normal mode. 

Thank you for help.

Re: Go to the View tab, and on the far left side of the ribbo...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ariel

 

 

seems that the form is somewhere out of the screen.

Have You worked with 2 screens in the last time?

 

Normally I only have one method to solve such issues:

 

I delete the Current User registry of the current Solid Edge version.

 

BUT: manipulating the registry ALWAYS is in behalf of Yourselve!

 

You can destroy Your installations doing it in a wrong way!

 

Besides this, rthere exists tools to move scrrens and windows out of actual visible area, but I have no experience with such tools

 

regards
Wolfgang

Re: Go to the View tab, and on the far left side of the ribbo...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I think you can limit your regedit to the toolbars key: HKEY_CURRENT_USER\Software\Unigraphic Solutions\Solid Edge\[Version in use]\Application\Toolbars

 

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200