Cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to increase the font size of the tree

Experimenter
Experimenter

I want change Font size of the tree...

I want to have a bigger font

Please help me.

Thank you.

2019-06-17 12_19_28-Window.jpg

6 REPLIES 6
Highlighted

Re: I would like to increase the font size of the tree

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Bobo76 You will have to change your Windows scaling to change the font size of Pathfinder tree.  Doing so will change the scale of everthing though, not just the Pathfinder tree...

 

There is a way to change it behind the scenes by hacking the registry, but that is not recommended as editing the registry directly can cause the application to fail or your PC to fail to boot, so use at your own risk.

Located in:  Computer\HKEY_CURRENT_USER\Software\Siemens\Solid Edge\Version 219\DEBUG

 

You will need to change the highlighted together to get it to look right.  As you increase the font size, the Item Size nneds increased to fit it, and then the spacing needs changed so that they don't run together in the tree.

 

2019-06-17_10-15-31.png



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: I would like to increase the font size of the tree

Experimenter
Experimenter
I didn't find anything about the fonts in the registers
2019-06-19 12_30_40-Window.jpg

Re: I would like to increase the font size of the tree

Phenom
Phenom

You need to open the "version 110" folder. Smiley Wink

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Re: I would like to increase the font size of the tree

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Bobo76 

 

 

 

as mentioned by @KennyG  You have to go to

 

 

Located in:  Computer\HKEY_CURRENT_USER\Software\Siemens\Solid Edge\Version 219\DEBUG

 

Your picture just shows the root of the Solid Edge tree

 

 

regards
Wolfgang

Re: I would like to increase the font size of the tree

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Bobo76 

 

 

and PS.: of course  this info has made me extremely interested, and Yes, of course, I immedeately have tried it.

And Yes, it works

 

 

regards
Wolfgang

Re: I would like to increase the font size of the tree

Experimenter
Experimenter

2019-07-01 09_38_07-Window.jpg

 

Thank you

It works perfectly.Smiley Happy