Cancel
Showing results for 
Search instead for 
Did you mean: 

IGES Can't open and use in "CypCut Tube Laser Cutting Program"

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

I have problem in IGES Export to Laser cut program (CypCut Tube Laser Cutting).

It can’t see model when open iges form Solid Edge. But can see model when use iges form Solid work.

 

(view in My Videos)

5 REPLIES 5

Re: IGES Can't open and use in "CypCut Tube Laser Cutting Program"

Honored Contributor
Honored Contributor

Grasping at straws here, but what order (6th order, 22nd order, etc...) Nurb curves can the translation use, and what ordered nurb curves are in the model? If you export without the S shaped cuts, does it work?

Re: IGES Can't open and use in "CypCut Tube Laser Cutting Program"

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

This case is IGES Export form Solid Edge Can't use in CypCut Tube Laser Cutting program.

Re: IGES Can't open and use in "CypCut Tube Laser Cutting Program"

Siemens Phenom Siemens Phenom
Siemens Phenom

I don't know how it occurred but the file that you are opening in the video as the Solid Edge genereted IGES file does not appear to be a valid IGES file -- this is why the data can not be used.  Did you try importing the Solid Edge IGES file back into Solid Edge?

Re: IGES Can't open and use in "CypCut Tube Laser Cutting Program"

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Yes. Iges file,Can open in Solid Edge

Re: IGES Can't open and use in "CypCut Tube Laser Cutting Program"

Experimenter
Experimenter

Have you found a solution to the problem? I have the same problem with a customer.