Cancel
Showing results for 
Search instead for 
Did you mean: 

INSIGHT INSTALLATION

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello Everyone,

 

I'm having some doubts to install Insight. For example, according to the attached images: when is mentioned to chose in the Solid DVD "Insight Server 2010", where can I find this option?

 

Thx!

4 REPLIES 4

Re: INSIGHT INSTALLATION

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You should have a data management DVD in your package. It's there.

Edit: Or, assuming you have maintenance you can download it from the Siemens website. Path below is to the ST9 MP4 Insight _Server location.

https://download.industrysoftware.automation.siemens.com/solid_edge/ST9/Maintenance_Packs/MP04/Insig...

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: INSIGHT INSTALLATION

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Thank you bshand! I did it!

 

Just one more question if possible: what user I need to use to create my farm? I was doing as images attached exemplify.

 

Thx in advance!

Re: INSIGHT INSTALLATION

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

First, I don't think the second part of my answer the Siemens path was correct if that's just a patch for Insight Server. 

But to your current quandary, you are past the point where I would be on the phone with my VAR or GTAC.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: INSIGHT INSTALLATION

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

I can only recommend to talk to someone with know how in this area.

 

Setting up a server just with a chat in in a forum is challenging.

 

Is is not only about setting up the server it going further with configuration and data migration.

Access control is in more than 80% of our support cases an issue. This can be difficult and sometimes the user locked out themselves after misconfiguration.Smiley Happy

 

Stefan

smitsch@unitec.de
www.all4edge.de