Cancel
Showing results for 
Search instead for 
Did you mean: 

IS ST8 AVAILABLE?

Genius
Genius

I just received a 2D Drafting Forum post (Selecting Multiple Objects to Move) that made reference to ST8 vs other versions.  This is the first time I've seen anything about an upgrade to ST7 being available. 

 

I did a search and found the system requirements for ST8, but is that for the free 2D version. If it is available since sometime in June, I guess I just missed email.  

 

Again, if available, I have a question re system requirements for ST8.  My computer meets all of the recommended requirements except that the display max setting is only 1920 x 1080.  Can I still download ST8 and what are the compromises that I will see. 

 

Thanks,

Ron

1 REPLY

Re: IS ST8 AVAILABLE?

MLombard
Retired

Yes, ST8 has been out for a few weeks now.

 

You should be able to handle ST8 with that hardware, but at that resolution, you might have to make some compromises in the display area, in particular the interface.

 

Best of luck!

Retired Community Manager for Solid Edge. This account is no longer active.