Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Icon

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

Hello,

When i create any assembly or any solid edge doc, the icon of it on my computer appears to be a black screen. I need to see the part or asssembly image as an icon.

Is there any settings for it?

Kindly help.

Thanks.

Regards,

Ashish Sarode

3 REPLIES 3

Re: Icon

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Hi Ashish:

 

From the Solid Edge Application menu, select Properties and from the Preview tab, create or save a preview. See if this helps.

 

~Tushar

Re: Icon

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @iashishsarode1,

 

I recall this was an issue early on, with Windows 10, which I assume you are seeing this on, ...and there was a maintenance pack, I don't rememember which one, that corrected it.

 

What SE version & MP are you using?....and which Windows version? 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP5] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Icon

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

My answer seems more like a workaround or quick fix.

Ashish you should really look into the suggestion by @SeanCresswell and get to the root-cause of the problem and check for the maintenance pack for a permanent solution.

 

~Tushar