Cancel
Showing results for 
Search instead for 
Did you mean: 

Identical Parts in Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I have parts that I would like to install in a different assemply. I tried the part under Parts Library not knowing what would happen, I found out that didn't work.

I tried >Modify< Transfer, I couldn't find the part to transfer.

Is there a way to assist.

 

Thank You

Greg

7 REPLIES

Re: Identical Parts in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Each part must reside in it's own PAR file which is then added to an assembly using the Parts Library pane in Edgebar in a ASM file.



Ken

Production: ST10 MP6
Testing: SE 2019

Re: Identical Parts in Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Could you rexplain: What a PAR and Edgebar? Solid Edge help will not open contains error.

 

Thank You

Greg

Re: Identical Parts in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg, the Help server is back up now.

 

A PAR is a Solid Edge Part file, so lets say I create a part model, I save it to disk as "1234.PAR" and close the file.

 

I then create a Solid Edge Assembly file (ASM file extension) and save it as XYZ.ASM and then I open the Parts Library tab on the EdgeBar (on the side of the Solid Edge graphics screen) and I navigate to the location I saved 1234.PAR and then I drag it in from the Parts Library pane into the assembly graphics window.

 

I have now placed 1234.PAR as a component of assembly XYZ.ASM



Ken

Production: ST10 MP6
Testing: SE 2019

Re: Identical Parts in Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

Ken,

I've opened up a new file the under local disk (C). I set to the assembly isolated the part to transfer under the new file folder. Came across Under numerous documents.

I,ve tried numerous times same results .

Is there any videos available to see?

 

Thank You

Greg 

Re: Identical Parts in Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Greg, here is a quick video showing...

  1. Creating a new part (Block_1.par)
  2. Saving it to the C:\Temp folde and closing it.
  3. Creating a new assembly (ASM_1.asm)
  4. Opening the Parts Library tab on EdgeBar
  5. Finding Block_1.par in C:\Temp
  6. Dragging it into the assembly (ASM_1.asm)
  7. Saving the assembly to c:\Temp and closing it.

 



Ken

Production: ST10 MP6
Testing: SE 2019

Re: Identical Parts in Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I got in to C/:temp fine getting into parts library is a difficult story.

As to the video never showed up. On Parts Library Shows Contacts to video.

 

http://screencast.com/t/3MvBTfO4A

 

Thank You

Greg

Re: Identical Parts in Assembly

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

have you try to check the view to show bar?

this could be the part view is not selected as the particular to be shown.

View.png

 

However if you want to input the same part which is exsist in assembly. you can just select it from the tree and drag drop it.

 

Thanks