Cancel
Showing results for 
Search instead for 
Did you mean: 

Identical Parts in Assembly

PLM World Member Valued Contributor PLM World Member Valued Contributor
PLM World Member Valued Contributor

I have 8 identical parts in an assembly using in a cutout. I would like edit the parts. So, I changed the parts names in pathfinder .

 

Thank you

Greg

1 REPLY

Re: Identical Parts in Assembly

Esteemed Contributor
Esteemed Contributor

If they are identical, then why did you need to change the names? BTW, changing them in pathfinder doesn't change the part file it will continue to point to.

 

You would need to right mouse click on each part [other than the first one] and choose from the "More" drop down menu, "Replace Part with Copy".

Then save each with a unique name....then you can create your cutout[s] either as an assembly-driven part feature[s], or as part feature[s]. You could even go into each part to make local edits to that part on it's own.

 

There are several ways to do many things in Solid Edge, but it does depend on the actual edit [cutout] you want to apply, as to how a particular process might be used.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP6] Classic [x2 seats]
Windows 10 - Quadro P2000