05-25-2015 08:01 PM
Dear Users,
When importing DXF files created using Illustrator the area fills are jagged and do follow the original splines. Circles however are properly filled. Also, DXF export in Illustrator seems duplicate the lines and splines. The fills are also seperate objects from the original drawing. Are these discrepancies par on the conversion process or
Is this a DXF limitation or a SE 2D display problem?
Regards,
Solved! Go to Solution.
05-26-2015 10:42 AM
Hi MariusMusicus I don't suspect that this problem is related to the display system in Draft. The problem is most likely related to the hatch boundary coming from Illustrator. The boundary may not have sufficient precision for SE to consider the boundary to be closed, or the boundary failed to translate successfully. If you would like to file an IR we can investigate this further.
05-30-2015 04:11 PM
Hi Steve W,
I opened the file using DraftSight free and the same problems occurs. Seems like it's an Illustrator export deficiency.
BTW, I'm very impressed with SE 2D. It's much easier to learn than DraftSight and slicker too. Great tools, thanks to Siemens for this software.
Regards,
Mario