Cancel
Showing results for 
Search instead for 
Did you mean: 

Image's Below the Plane

N/A

The three parts in this image http://screencast.com/t/145CspmNBjq shows that two parts are below the plane... were moved not like the part on the left. I moved the two parts not knowing that they would end up below the plane. What caused this? I've tried to move but I couldn't move.
This image is to illistrate in the pathfinder that there are three solid bodies inactive one active, there are three other Solid Bodies not shown are active. How to active all Solid Bodies. http://screencast.com/t/6OInVT5LQFG

Thanks
Crousie

1 REPLY

Re: Image's Below the Plane

Esteemed Contributor
Esteemed Contributor
You can only activate one body at a time.


Ken

Production: ST10 MP5
Testing: SE 2019