Cancel
Showing results for 
Search instead for 
Did you mean: 

Import file orientation

Pioneer
Pioneer

When I import a file, can I choose/change how it is oriented relative to the Base Reference Planes?  The .par file is curretly oriented like the image on the left, I want it to be oriented like the image on the right (see attached image).  That way, when I replace it, it will be in the same general location and orientation in the assemblies.

Gabriel Gullickson
Mechanical Drafter
Spectrum Industries
ST8
2 REPLIES

You cannot specify the orientation on import, but after i...

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You cannot specify the orientation on import, but after it is imported you can rotate it as needed in Synch mode.  Just turn off Live Rules and select everything.



Ken

Production: ST10 MP6
Testing: SE 2019

Re: You cannot specify the orientation on import, but after i...

Pioneer
Pioneer
Yes, it works. Thank you very much.
Gabriel Gullickson
Mechanical Drafter
Spectrum Industries
ST8