Cancel
Showing results for 
Search instead for 
Did you mean: 

Import other file types

Not applicable

Seems that the free version will not import ACIS, or IGS files. Always get a box
that says I don't have a translator for the file type. This does limit the usefulness
of this program for me as I get a lot of files from customers to quote and cannot
use Solid Edge 2D.
Also the program does not support intelligent blocks, that feature is also disabled.
Again, this is one of the more useful features of Autocad.
This is a Great product but it has been limited. I will need to stick with Autocad
until I can upgrade to the full version of Solid Edge.
Jerry
1 REPLY

Re: Import other file types

Not applicable
ACIS (SAT) is not a 2D format. It is a solid modeling format -- thus not
included in the 2D product. On IGS similar story -- IGES is mostly used for
3D these days. Its been largely displaced by DWG and DXF which are the
defacto standards in 2D drawing exchange. Your customers/suppliers should
all be able to supply DXF or DWG.
DS

"Jerry Tidell" wrote in message
news:4521c2fd$1@bbsnotes.ugs.com...
>
> Seems that the free version will not import ACIS, or IGS files. Always get
> a box
> that says I don't have a translator for the file type. This does limit the
> usefulness
> of this program for me as I get a lot of files from customers to quote and
> cannot
> use Solid Edge 2D.
>
> Also the program does not support intelligent blocks, that feature is also
> disabled.
> Again, this is one of the more useful features of Autocad.
>
> This is a Great product but it has been limited. I will need to stick with
> Autocad
> until I can upgrade to the full version of Solid Edge.
>
> Jerry