Cancel
Showing results for 
Search instead for 
Did you mean: 

Import part and end up with one solid body.

Legend
Legend

Hi,

 

Is there a way to import parts from third parties, and end up with a single body..

 

I have attached an example of a motor..  have a look..

 

Kind Regards

 

 

Jan Bos

2 REPLIES 2
Highlighted

Re: Import part and end up with one solid body.

Siemens Legend Siemens Legend
Siemens Legend

This model is actually pretty clean and might boolean into a single solid but even then it has way to much detail which will carry over into drawings etc. (Do you really need the fins and the vent coolling holes in the back, the text on the top?)

 

Most often supplier parts have WAY to much detail in them where all you need are the overall dimensions, shaft location/size and mounting locations.

 

For Assemblies like this I place them in an ASM and Create a new part in place.
I then model using Sync to create a simplified rep. (Sync Extrude, Boolean, replace face etc.)

to get what I want.

 

This works well for parts like this and also works when it is a true ASM. If you are running managed you can create a single part and check that in rather than checking in 100's of files (Perhaps) that make up the componet you really treat as a single part in your design.

 

Again, I don't try to "fix" the imported geometry which can take hours. I use this to make a new part that is a clean single solid. Taking a few minutes to do this can yield some nice results.

See attached.

 

Hope this helps

 

Thanks,

 

Art

 

 

 

Re: Import part and end up with one solid body.

Legend
Legend

Hi Art,

 

You are right this is the way to go.. simplfy it..

 

Thanks for your input.

 

Reg.

 


Jan Bos