Cancel
Showing results for 
Search instead for 
Did you mean: 

Improvement to level control when sketching

Gears Phenom Gears Phenom
Gears Phenom

Hello,

 

There have been a lot of discussions in the past about improving the level control when sketching. I would like to see an improvement when picking the active level.  Instead having to right click on the desired level and picking "make active", it would be more efficient to just click on that level have it become active.  Highlighting in red would help identify it quickly.  I use Corel Draw for silkscreen artwork and this is how it's set up.  This reduces mouse click.

 

Kyle

Kyle Joiner
IPA LLC
ST10 MP1
3 REPLIES

Re: Improvement to level control when sketching

Community Manager Community Manager
Community Manager

Can't use single click, since that is select and some things are object action. That said, I believe DOUBLE CLICK is the way you can activate a layer today.

 

Dan Staples
Director, Solid Edge Product Development

Re: Improvement to level control when sketching

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Dan is correct, a double click activates a layer...



Ken
Production: ST10 MP7, Testing: SE 2019
http://Grundey.blogspot.com

Re: Improvement to level control when sketching

Gears Phenom Gears Phenom
Gears Phenom
Thanks Dan! That works great.
Kyle Joiner
IPA LLC
ST10 MP1