Cancel
Showing results for 
Search instead for 
Did you mean: 

Inquire part level hole from assembly

Can anyone running ST7 confirm if the new Measure tools can do this?

 

Or if there is any other method im not aware of...

 

From the assembly I want to inquire holes in a part...  I can place a PMI dimension or inquire the element and get it's diameter but I want to know if its a tapped hole ot just a thru hole...

 

Is there any method for doing so?   I tried placing a PMI call out with %HC but this did not return anything.???

 

Something i've missed all these years or anything new in ST7?

 

Please and Thank you!

 

4 REPLIES

Re: Inquire part level hole from assembly

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Matt, yes you can do this with new Measure command from assy level to part and vice versa.

 

Here is a video:

 

You can do this from Callout too, but fileds should contain codes (%XX) on Feature Callout tab! This works only "active level"!

 

BR, 

Imics
http://solidedgest.wordpress.com/

Re: Inquire part level hole from assembly

Thanks Imics,

 

Does this work for ordered parts too?  I can not "read" your pathfinder to know if that was an ordered or Sync part.

 

It's ordered hole features that we want to inquire from the assy...

 

thanks much

 

Re: Inquire part level hole from assembly

Gears Phenom Gears Phenom
Gears Phenom

Matt,

 

Yes, it works for both methods! (stupid Hungarian UI Smiley Happy )!

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Inquire part level hole from assembly

Thank you Sir!!!