Cancel
Showing results for 
Search instead for 
Did you mean: 

Inseritng components ( part, assembly ) To assembly

Pioneer
Pioneer

Hello

 

In SW I very often maked some operation:

Dividing display into 2 windows. On the right side I've opened some assambly. From left side I've opened another one assembly or part.

So , when I want  to insert part or assembly from left window to assembly in right window I need only to drag and drop it to window on right side.

In SE I can not do this ( drag and drop opened part or assembly document  from window to window)

 In SE I have to click "insert component" and then I need to find the right path. When I will find right path then I have to find right document ( filename). It takes much more time than drag and drop.

 

Anybody know any similar method to this in SW.

 

Regards

Marcin

2 REPLIES

Re: Inseritng components ( part, assembly ) To assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You can select "open documents" in the parts library and you will get a list of any open SE par, asm, psm file which you can drag and drop.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200

Re: Inseritng components ( part, assembly ) To assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I guess it's worth mentioning that you can also tile windows of assemblies and use copy and paste of parts and subassemblies from one to the other.

Bruce Shand
SE2019 MP4 - Insight - Win10 - K4200