Cancel
Showing results for 
Search instead for 
Did you mean: 

Insight ST9 FYI

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

With Insight ST9 you must install the Insight Client component or you will not see the Manage tab in the Solid Edge options.

In the past some customers had avoided installing this unless they needed the enable logging feature.

And if your license does not have the Insight feature for some reason you also will not see the Manage tab in Options.

LMGi
www.TLMGi.com
1 REPLY 1

Re: Insight ST9 FYI

Gears Phenom Gears Phenom
Gears Phenom
During ST9 beta test I discovered that if you use a personalized theme from a previous version the Manage Tab is not automatically added\shown.

I found this strange cause new features\tolls are automaticcally added in the ribbon even when you use a previous version theme.

I have then logged an IR explaining that users would be confused and\or totally miss the manage tab.
Apparently I was the only that worried about it and the IR was closed as an ER.


IR 7728057 has been converted to PR 7728057; Desc: ST9 Beta: Management Tab hidden by default when coming from a personalized theme