03-09-2018 08:59 AM - edited 03-09-2018 09:01 AM
We use Solid Edge ST9 with insight and use life cycle assistant when revising files.
We have an Engineering Change group in Sharepoint with the standard permission level "Contribute" on the released library in sharepoint. That however gives the users permission to delete files as well in that library which I do not want. So I created a new permission level in sharepoint that is the same as “Contribute” but without the delete permission.
So far so good, but when I run LCA on a file and LCA wants to move the released file to the obsolete library I get an error message: “Delete permission must be added to the library for “user”.”
So what is the best permission setup when working with pre-released/released/obsolete librarys and in Insight?
Any help is appreciated!
03-09-2018 10:29 AM