02-02-2018 01:32 PM - edited 02-02-2018 01:38 PM
Hello everyone,
I have issue when I try to get the area of a sketch. It grays in the area of the sketch but no "value" shows up. I have multiple screens but appears it's not hidden on them. I checked a co-workers and it works fine for him. Running ST10 SP3 on Window 10 with a Nvidia Quadro K2100M.
Any suggestions?
Thanks,
Matt W.
Update: Only happens in part. I copied sketch to draft and was able to get my numbers.
Solved! Go to Solution.
02-02-2018 01:37 PM
Hi @cadnerd
have You tried to rename the Current User Registry path for Solid Edge v110 to get a default setting.
So You can see wether it is a general issue or a failure from personal settings.
Also all form positions will be reseted to standard values.
PS.: have You changed any monitor options in the last time?
Dual, Mono screen, resolution, etc.
02-02-2018 01:41 PM
No I don't mess with the registry, cause I'll probably screw something up.
Nope same monitors and settings I've have for almost a year now.
02-03-2018 07:52 AM
Hi,
I think this is a graphic driver problem.
Switched to "software" in Display options and the text reappears.
I don't think this problem arises by registry entry, since no window is used to display the value at the cursor.
02-05-2018 01:26 PM
Thanks JB! You nailed it. I tried all the settings and only "software driven" worked as expected. Should've known it was the graphics card.
Thanks for everyone's help.
Matt W.