Cancel
Showing results for 
Search instead for 
Did you mean: 

Inspect Obtuse Angle Results

Creator
Creator

Couldn't help but notice over the past 2 years that ST6 would not give a straight readout when measuring an obtuse angle in the part/assembly environment.  Just upgraded to ST10.  Problem still appears.  Does anyone know if maybe I'm using the tool wrong?  Other modeling softwares seem to tackle this with ease.  For some reason with Sold Edge I'm stuck doing more math after the command.

Capture.PNGThe angle is actually 195 between the two planes.Capture 3.PNGWhat the * does this mean?

3 REPLIES 3

Re: Inspect Obtuse Angle Results

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

I suggest using Measure command with Angle option... It's a smart solution.

 

 

BR,

 

 

Imics
http://solidedgest.wordpress.com/

Re: Inspect Obtuse Angle Results

Creator
Creator

That seems to work.  Not sure why the "inspect angle" button doesn't work the same.

Re: Inspect Obtuse Angle Results

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ATonellato

 

 

 

as mentioned and suggested already by @Imics to use the SmartMeasure tool would always be the best.

 

The result of the old angluar measurment is the angle between the two surface normals.

So this is/was an old mathematical approach using vector algebra as in my very old times.

 

But of course this alone must not be the excuse of deliver the smalle angle between those two planes

 

regards
Wolfgang