Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation Issues (Previous Version of Solid Edge on Machine)

N/A

Every time I try to install Solid Edge on my computer I get an error message stating that I already have a previous version of solid edge installed on my computer and to uninstall it using Programs and Features. Solid edge is not a program installed on my computer nor is there any program files on my C drive for it.

I did try to install the program a few weeks ago but the installation failed half way through.

I was just wondering what I can do to correct this issue.

1 REPLY

Re: Installation Issues (Previous Version of Solid Edge on Machine)

Siemens Phenom Siemens Phenom
Siemens Phenom
Here are the steps to manually uninstall and clean up any Solid Edge
installed software:
1. Uninstall the Solid Edge software using Add/Remove Programs.
2. Manually delete the Solid Edge program folders typically in
C:\Program Files and/or C:\Program Files (X86).
3. Manually delete the Solid Edge user preference folder
%APPDATA%\Unigraphics Solutions.
4. Manually clean up the registry by deleting any Solid Edge registries
in the following locations:
HKEY_CURRENT_USER\Software\Unigraphics Solutions
HKEY_LOCAL_MACHINE\Software\Unigraphics Solutions
HKEY_LOCAL_MACHINE\Software\Wow6432Node\Unigraphics Solutions
5. Reboot the workstation.
6. Attempt to reinstall the software again.

-Dave
On 15/02/2013 02:45, jpwmcneill@gmail.com wrote:
>
> Every time I try to install Solid Edge on my computer I get an error
> message stating that I already have a previous version of solid edge
> installed on my computer and to uninstall it using Programs and
> Features. Solid edge is not a program installed on my computer nor is
> there any program files on my C drive for it.
>
> I did try to install the program a few weeks ago but the installation
> failed half way through.
>
> I was just wondering what I can do to correct this issue.
>
>