Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation Problem

Experimenter
Experimenter

I have a problem installing solid edge st10.

I tried to completely uninstall solid edge st6 and install solid edge st10 but when i try to run the setup, this pops up

Knipsel.PNG

I can't find any more files of solid edge st6...

please help

5 REPLIES 5

Re: Installation Problem

Gears Phenom Gears Phenom
Gears Phenom

 

I do not know how the Student Install files are delivered...   BUT, look for "SECleanupAll.exe" in a folder called at [InstallFolderLocation]\Solid Edge\ST10\64-bit\DVD\Solid Edge\SptTools\SECleanup


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Installation Problem

Experimenter
Experimenter
Thanks for the response but i did that already, the setup file for st10 is just one file and if you click on it, it starts it but then i get that error

Re: Installation Problem

Gears Phenom Gears Phenom
Gears Phenom

Per @uk_dave from a different thread (Ref HERE)

 

<SNIP>

Within the trial download folder C:\SEWebInstall should be the twenty 7-Zip files and also a Solid_Edge_Web_Package_ST10.exe file.

 

Double-click on this Solid_Edge_Web_Package_ST10.exe and your twenty files will automagically be extracted into  a Solid Edge media install folder C:\SEWebInstall\Solid Edge.

<END SNIP>

 

Once Extracted, look for the SECleanupALL tool


Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Installation Problem

Siemens Phenom Siemens Phenom
Siemens Phenom

From GTAC Solution Center article 002-7007115:

 

  • Symptom
    ---------------
    Sometimes after uninstalling Solid Edge software products and then attempting 
    to reinstall Solid Edge software you receive an error message "Another 
    version of Solid Edge is already installed".
  • Hardware/Software Configuration
    Solid Edge
  • Solution
    This indicates that the previously uninstalled Solid Edge software was not 
    properly removed requiring a manual uninstall and clean-up of the Solid 
    Edge software.	To manually uninstall and clean-up Solid Edge software:
    
    1. Uninstall the Solid Edge software using Add/Remove Programs.
    
    2. Manually delete the Solid Edge program folders typically in C:\Program 
    Files.
    
    3. Manually delete the Solid Edge user preference folder 
    %APPDATA%\Unigraphics Solutions.
    
    4. Manually clean up the registry by deleting any Solid Edge registries in 
    the following locations:
    
        * HKEY_CURRENT_USER\Software\Unigraphics Solutions
    
        * HKEY_LOCAL_MACHINE\Software\Unigraphics Solutions
    
        * HKEY_LOCAL_MACHINE\Software\Wow6432Node\Unigraphics Solutions
    
    NOTE!  There may be other Siemens PLM software installed under the 
    "Unigraphics Solutions" locations.  Take care to not delete these entries 
    and only remove Solid Edge related entries.
    
    5. Reboot the workstation.
    
    6. Attempt to reinstall the software again.

Re: Installation Problem

Gears Phenom Gears Phenom
Gears Phenom
Thanks, Dave!

Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
SE2019 Pre-Production Testing
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7