Cancel
Showing results for 
Search instead for 
Did you mean: 

Installation problem

Not applicable
Hi,
I have Solid Edge ST3 MP3 in french installed on XP SP3. I wanted to try SE 2D ST3 Free for fun so I downloaded the french version but, the installation wizard tells me that a version of Solid Edge is already installed and that I need to un-install it before continuing the installlation of SE 2D ST3 Free. Now I obviously don't want to un-install SE ST3 to get 2D Free, but is it necessary? If not how can I fix the problem.

Thank you

-Max
1 REPLY

Re: Installation problem

Not applicable
This is true.
You cannot have Solid Edge and Solid Edge 2D Drafting loaded at the same
time.
Both softwares use the same registry entries.
Regards,
Rick B.
"dufresne.maxime@gmail.com"

wrote in message
news:dufresne.maximegmail.com.4v2hwz@noreply.bbs.industrysoftware.automation.siemens.com...
>
> Hi,
> I have Solid Edge ST3 MP3 in french installed on XP SP3. I wanted to try
> SE 2D ST3 Free for fun so I downloaded the french version but, the
> installation wizard tells me that a version of Solid Edge is already
> installed and that I need to un-install it before continuing the
> installlation of SE 2D ST3 Free. Now I obviously don't want to
> un-install SE ST3 to get 2D Free, but is it necessary? If not how can I
> fix the problem.
>
> Thank you
>
> -Max
>
>
> --
> dufresne.maxime@gmail.com
> ------------------------------------------------------------------------
> dufresne.maxime@gmail.com's Profile:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/member.php?userid=331031
> View this thread:
> http://bbs.industrysoftware.automation.siemens.com/vbulletin/showthread.php?t=45641
>