Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Installing Solid Edge and the license

Not applicable
I don't know how to transfer it Smiley Frustrated was going to ask my lecturer tomorrow, but I don't know if he'll know

Re: Installing Solid Edge and the license

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I would suggest you make yourself a copy of the license & SolidEdgeV104ENGLISH_32Bit.exe files to a DVD, or flash drive....to have on hand for re-installation, or even passing on to your friends.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Installing Solid Edge and the license

Not applicable
Hey guys,

I have got an e-mail, that i should have installed Solid Edge. But it isn't right now.
I didnt get any download link to my email.

Is there any chance to get a new download-link for Solid-Edge ST-4?

best regards

Re: Installing Solid Edge and the license

Not applicable
Check your Junk folder to insure it didn't go there. You can also go
back and fill the form out again to get it to resend you the link. If
you search the forum, somebody was posting a direct link to download it too.
Ken
http://grundey.blogspot.com
http://www.pella.com

On 10/22/2011 6:09 AM, Achim_Wawer@web.de wrote:
> Hey guys,
>
> I have got an e-mail, that i should have installed Solid Edge. But it
> isn't right now.
> I didnt get any download link to my email.
>
> Is there any chance to get a new download-link for Solid-Edge ST-4?
>
> best regards
>
>

Re: Installing Solid Edge and the license

Not applicable
I also just installed the software, but after the solid edge splash screen, I get "Engine Error" 'The application is not properly registered. You may need to reinstall it.' I just reinstalled and got the same error message. Any ideas?

Re: Installing Solid Edge and the license

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
I also just installed the software, but after the solid edge splash screen, I get "Engine Error" 'The application is not properly registered. You may need to reinstall it.' I just reinstalled and got the same error message. Any ideas?



Hi there,

Sounds like a corrupt exe file....but sometimes it's hardware / drivers / opertaing system, or a combination of, so it would help narrow it down with this information.

-
Such as mine.....
OS: Win7-x64 SP1
Computer: Custom built
CPU: i7 930 @2.8GHz
RAM: 12GB
Graphics & Driver: Quadro FX1700 / 267.79
Primary HDD: 100GB-SSD
-
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Installing Solid Edge and the license

Not applicable
Hi,
I installed ST4, it came up with the license error so i uninstalled and attempted to re install thinking that would solve the problem but it just comes up with an error message saying that there is already a version installed... but there isn't, i cant find it anywhere...

Any help would be much appreciated

Cheers

James

Re: Installing Solid Edge and the license

Not applicable
Hi everyone,

by the installing process everything is OK.
When I have started my first project the "Solids" model (Extrude, Revolve, etc.) isn`t active.
Could anyone help me?
Txs in advance.

Re: Installing Solid Edge and the license

Not applicable
If you are in the Synch mode (default), those commands will be inactive
until some sketch geometry is created first.
Ken
http://grundey.blogspot.com
http://www.pella.com

On 11/9/2011 3:06 PM, yordanov.martin@abv.bg wrote:
> Hi everyone,
>
> by the installing process everything is OK.
> When I have started my first project the "Solids" model (Extrude,
> Revolve, etc.) isn`t active.
> Could anyone help me?
> Txs in advance.
>
>

Re: Installing Solid Edge and the license

Not applicable
Hi I received the email with the link but every time I tried opening the link it would refuse. I am using windows 7 32 bit