Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: Installing Solid Edge and the license

Not applicable
Hey,
I've a problem with my ST4. I've installed the ST4. When I open the program it lecks very long and nothing go on.

I have a ASUS n73S with Windows7 Home Premium 64bit.

Is the program only for a 32Bit Windows?

Thanks for answers

Ralfi

Re: Installing Solid Edge and the license

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
The program is 32 bit but runs just fine on Win7 64 bit. It is best to make sure you right mouse click on Setup.exe and choose Run As Administrator when installing. If you did not do this it would be worth removing the application and reinstalling using this method.


Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Installing Solid Edge and the license

Not applicable
So I have done what you have said. The program runs Smiley Happy. Thanks for the quick help.

Re: Installing Solid Edge and the license

Experimenter
Experimenter
Hello i have been messaging to everyone and asking about my problm but no one answered. I downloaded directly from the siemens website and when i got confirm your email message i confirmed it but i have not received any license file or academic code in email plz help me

Re: Installing Solid Edge and the license

Siemens Phenom Siemens Phenom
Siemens Phenom

@Sujata please do not cross post the same question across forums.  Your question is currently being actively worked under your other posting:

 

https://community.plm.automation.siemens.com/t5/Solid-Edge-Forum/License-file-not-received-till-now/...