Cancel
Showing results for 
Search instead for 
Did you mean: 

Installing problem on a 32bit computer

Experimenter
Experimenter

A successful download for 2D Drafting but when I come to install the only installation program is for the TS8 release, which as my computer is a 32 bit system will not load.  How do I resolve this problem?

2 REPLIES

Re: Installing problem on a 32bit computer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

ST8 is 64 bit only.  You will have to get ST6 as it was the last 32 bit version.  Not sure how to go about that as I don't see it avaialble on the Free 2D site.



Ken
Production: ST10 MP9, Testing: SE 2019
http://Grundey.blogspot.com

Re: Installing problem on a 32bit computer

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

As @KennyG says, you'll need to run ST6 on your 32bit Windows.

One of the Siemens admins will likely see this thread and make contact directly, with a link to download the ST6 version.

 

Alternatively, if it's an option, you could upgrade [or indeed replace] your system to a 64bit version of Windows.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP1] Classic [x3 seats]
Windows 10 - Quadro P2000