Cancel
Showing results for 
Search instead for 
Did you mean: 

Internal Volume

Genius
Genius

Hi guys.

 

I have a gearcase with internal profile witn pockets.

How do I calculate the internal volume?

 

I am running ST7.

5 REPLIES

Re: Internal Volume

Gears Phenom Gears Phenom
Gears Phenom

there are a few methods...

 

1.) boolean to get the internal volume

 

2.) revolve an open profile 

 

in either case, you will want to take advantage of multibody support ...

 

 

===================================================
Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.7

Re: Internal Volume

Genius
Genius

Hi Matt.

 

Is there training on this because I don't know how to do it?

Re: Internal Volume

Pioneer
Pioneer

hey @Dazzie

 

There are lot of videos available on Youtube.

 

please find below link.

 

https://www.youtube.com/watch?v=uHtFIiI42N0

 

hope it will help you..

Re: Internal Volume

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

There are some ways to get internal volume, I like to use Delete regions command.

 

Here is a video about steps:

 

I hope this helps.

 

BR,

Imics
http://solidedgest.wordpress.com/

Re: Internal Volume

Genius
Genius

Hi Harsh9592

 

Thanks for the link.

 

Helped lots.

 

The only issue I had was when I had to BOUND the edge as it was profiled.

Because I wanted to know the volume for and oil quantity I cut the box down to the max level and then I was able to BOUND the edge.

 

Worked a treat.