Internal volume

Valued Contributor
Valued Contributor

Ideally, I would like to find the internal volume of some pipes in an assembly.  It doesn't look like it would be possible so my next choice is to measure the internal volume of individual pipe segments and add them.

 

I followed a method to use the internal surface of the pipe to create a new solid body and measure its volume.  I followed the steps and was able to create a solid body of the internal volume, but the measured volume doesn't seem right.  I usded the Surfacinc copy command to copy the internal volume and then used Bounded options to close both ends and finally stitch them all into a single solid body.

 

The radius is 0.44" and the lenght is 135" and the volume should be around 82 cubic inches, but the volume shows is 23.92, which is the same as the volume of the material of the pipe I started with.

 

I probably made a silly mistake somewhere and my brain is too tired to figure it out.

 

Thank you.

Ali

14 REPLIES

Re: Internal volume

Esteemed Contributor
Esteemed Contributor

This is what I get:

 

tubevol.JPG

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Internal volume

Esteemed Contributor
Esteemed Contributor

If you were using Physical Properties to measure it, it only works on the Design Body whether displayed or not.  Your cylinder was a Construction Body.  You have to measure it like @bshand did.



Ken

Production: ST10 MP3
Testing: SE 2019

Re: Internal volume

Esteemed Contributor
Esteemed Contributor

Yeah, so if you toggle solid body_7 to design and design body_1 to construction the properties will give you the volume of the design body representing the internal volume. I learned something here...

Edit: No, I'm wrong here. No need to toggle. Just make sure the right one is selected.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Internal volume

Valued Contributor
Valued Contributor

This is exactly what I need.  Can you please tell me what command I should use?

 

Also, can you please tell me how you would toggle construction/physical bodies?

Re: Internal volume

Siemens Phenom Siemens Phenom
Siemens Phenom

The Measure command on the Inspect tab will give you the results that @bshand posted.

 

Greg

Re: Internal volume

Valued Contributor
Valued Contributor

I already tried that, but it doesn't give the volume.0measures.png

Re: Internal volume

Esteemed Contributor
Esteemed Contributor

Go to the options in the measure dialog to add volume.

Right click a body and you will see the toggle command.

Bruce Shand
ST10 MP3 - Insight - Win10 - K4200

Re: Internal volume

Siemens Phenom Siemens Phenom
Siemens Phenom

Set the Element Type filter to Solid Bodies instead of All Elements and it will give you the desired results.

 

measure.png

 

Re: Internal volume

Valued Contributor
Valued Contributor

I checked the options and all the measurements are checked.  Am I clicking on the right options box?

0option.png