Cancel
Showing results for 
Search instead for 
Did you mean: 

Invalid license file syntax

Not applicable
I downloaded the program and everything installed fine. I went to License Utility and selected browse to find SElicense.dat following path My Computer>CSmiley EmbarassedProgram Files>Solid Edge ST4>Program>SELicense. I click ok and the program closes. I go to ope Solid edge and I get a pop up dialog box that says:

SOLID EDGE LICENSE CHECK

A connection to the file server could not be establishes. Contact your system administrator to resolve the connection to the server.

Invalid License file syntax.
Feature: server_id
License path: C:\Program files\Solid Edge ST4\Program\SELicense.dat;
FLEXnet Licensing error:-2,413
For further information, refer to the FLEXnet Licencing Documentation, available at "www.flexerasoftware.com

Please advise
8 REPLIES 8

Re: Invalid license file syntax

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Hi Ryan,
The directory you state, is the install path.....the existing license file is like a place holder for Solid Edge to look for at every start-up.
The correct file will be in the email you got, as an attachment, and should have the same exact name.
So close.... Smiley Very Happy
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Invalid license file syntax

Not applicable
Leave it to an engineer to over complicate things!!! thank you so much!

Re: Invalid license file syntax

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor
Haha, yeah,...and it's when "we" do that shennanigans to our own things, it really gets annoying. Smiley Wink
You're most welcome...enjoy.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP7] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Invalid license file syntax

Experimenter
Experimenter

I receive an error message saying I don't have any valid Solid Edge Licenses. I used the SElicense.dat file I received via email and put in the program folder of the drive that the folder is on. My setup is Node locked and is an at HOME USE license. But My computer updated just the yesterday and since, I have been unable to open solid edge. However for up to the minute prior to my system update, and three months prior I had zero issues. 

 

adaniels@esmetals.com

Re: Invalid license file syntax

Siemens Phenom Siemens Phenom
Siemens Phenom

@SMF-ST8-1989 firstly I think a  new thread would have been more appropriate for your question.

 

With that said have you opened your selicense.dat file into a text editor and checked the Solid Edge version, the SE CID,  and the expiry date?

Re: Invalid license file syntax

Experimenter
Experimenter
INCREMENT solidedgeclassic selmd 108.0 29-nov-2017 uncounted \
VENDOR_STRING="SOLID EDGE HOME USE" \
HOSTID=COMPOSITE=41CFBCFEBC3A SIGN="16ED BDC0 381F 5966 0B2F \
D8CD EA6C B508 5A45 E5ED 0B1A 542C 73F8 8167 FCBE 0DB3 4701 \
6F70 AB24 D9A3 06BE 7789 B6D2 854C 9134 07CF 4D2E 20B3 5E6A \
8AD1"

Anthony (Tony) Daniels / Drafter
adaniels@esmetals.com / 913-674-6951
Ernest-Spencer Metals inc.
Office: 785-484-3165 ext 214 / Fax: 785-484-3208
3323 E 82nd street Meriden, KS 66512
http://ErnestSpencer.com
Highlighted

Re: Invalid license file syntax

Siemens Phenom Siemens Phenom
Siemens Phenom

And you are currently running ST8?

Re: Invalid license file syntax

Siemens Phenom Siemens Phenom
Siemens Phenom

Also, run the Solid Edge License Utility and check your SE CID in the to[ right-hand corner.  Is it showing as 41CFBCFEBC3A?  If not then your SE CID has changed.

 

If the version, date, or SE CID in the license do not match as expected then you will need to regenerate your home use license.