Cancel
Showing results for 
Search instead for 
Did you mean: 

Is There a Full Three Point Radius Feature?

Valued Contributor
Valued Contributor

I'm trying to make a full root radius on a gear tooth.  Solidworks has this feature.  Is there a way to do this in Solid Edge?  This is just a round tangent on three sides.

 

Thanks,

 

Matt

3 REPLIES

Re: Is There a Full Three Point Radius Feature?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I don't believe so.  3 point arc that you can extrude, but not a dedicated round.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Is There a Full Three Point Radius Feature?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MattS

 

I think there is only the way to first create a circle and afterwards put the tangent relations onto it.

 

regards
Wolfgang

Betreff: Is There a Full Three Point Radius Feature?

Valued Contributor
Valued Contributor

Thanks.