Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible, to access the "quantity" field that is available in assembly "reports" function?

Creator
Creator

I would like to access the "quantity" field that is available in the assembly reports function; ideally I would like to see it in the variable table. What I would like to do is take an item's surface area and multiply it by the quantity of those parts in an assembly.

3 REPLIES 3

Re: Is it possible, to access the "quantity" field that is available in assembly "rep

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

Not sure abou the variable table but I could pull the quantity value in a callout.

Select Callout - Properties - Property Text - Select the Part from the Tree - From Graphic Conection - Parts List Quantity - Select - OK - OK

%{Parts List Quantity|G}

 

 

The Surface area can also be found under the Graphic Connection list.

%{Surface Area|G}

 

Unfortuately these cannot be multipled nor the Variable table accepts these as Formulas.

 

Tushar Suradkar

http://surfandcode.blogspot.in

 

Re: Is it possible, to access the "quantity" field that is available in assembly "rep

Gears Phenom Gears Phenom
Gears Phenom

Hi,

 

Here is a video about this:

 

You have to toogle on surface area in variable table on part level.

 

I hope this will help you.

 

BR,

Imi

Imics
http://solidedgest.wordpress.com/

Re: Is it possible, to access the "quantity" field that is available in assembly "rep

MLombard
Retired

Great looking model. CAD doesn't have to look boring.

Retired Community Manager for Solid Edge. This account is no longer active.