Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to replace a part with another in draft?

Creator
Creator

Hey,

 

I made 2 sheets in draft and place the same part on both of them (one link!). Is it possible to "replace" one part on one sheet so that the second sheet is not affected?

2 REPLIES

Re: Is it possible to replace a part with another in draft?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

No.  The access to the link where this can be edited sees all views pointing to the same model as one link.  You will have to delete and recreate the view to the different model file.



Ken

Production: ST10 MP7
Testing: SE 2019
http://Grundey.blogspot.com
Highlighted

Re: Is it possible to replace a part with another in draft?

Creator
Creator
Thanks for Your answer. Sad to hear that but now I know that it has to be done the right way from the beginning =)