Cancel
Showing results for 
Search instead for 
Did you mean: 

Is it possible to search for a part or assembly looking for the "Title" file property?

Gears Phenom Gears Phenom
Gears Phenom

I'm needing to find some particular files on our server, and they have the file properties filled out, however a simple windows search has done no good. We don't use insight or teamcenter, is there any way for us to find these files through a search for keywords?

Solid Edge 2019
Windows 7 Professional
Nvidia K2200 & Intel Xeon
"You're doing it wrong"
5 REPLIES 5

Re: Is it possible to search for a part or assembly looking for the "Title" file property?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Looks like this may help:

https://msdn.microsoft.com/en-us/library/aa965711(v=vs.85).aspx

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Betreff: Is it possible to search for a part or assembly looking for the "Title" file prop

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi,

 

 

 

 

have You seen the following video about the new ST9 Data Managment Capabilities:

 

http://www.plm.automation.siemens.com/en_us/products/solid-edge/st9/index.shtml#lightview%26url=http... Edge ST9%26description=Built-in Data Management%26width=800.0%26height=450.0%26fullscreen=true%26autoplay=true%26docType=mp4

 

 

There You can see the search functions from windows explorer using indexed Solid Edge properties.

 

Maybe it helps

 

regards
Wolfgang

Betreff: Is it possible to search for a part or assembly looking for the "Title" file prop

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Since windows explorer usually has the first and most important column of "name" simply using something in the search box like "name:motor" (without quotes) finds any file with "motor" in the name. Additionally, say the file also had "50hp" somewhere in the name. So then you would put "name:motor name:50", etc.

Right click on a column to see the many properties possible.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Is it possible to search for a part or assembly looking for the "Title" file property?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If you use the Solid Edge Search found on the Open form, you can specify "Title" as a search field and then specify the search string.

 

If your files reside on a Windows server and they are indexed by Windows Search, then in the Explorer search field, use:  title: "string to search for"



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Is it possible to search for a part or assembly looking for the "Title" file property?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@KennyG, I hadn't thought of that. I think because I've been on Insight so long I wrongly think of that search as an Insight thing.

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200