Cancel
Showing results for 
Search instead for 
Did you mean: 

Is the hole feature limited to size?

Valued Contributor
Valued Contributor

I'm using the hole cut feature in my model. It's default size is 10mm - when i add a dim to the hole sketch and try to change it to 100mm it doesnt like that and just changes the callout to 100mm, but not the actual size. 

 

should i be using cut instead of hole, due to its large size?

 

 

Regards,

MagRiz
(ST9 User Est 01.18)
1 REPLY 1

Betreff: Is the hole feature limited to size?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @MagRiz

 

 

 

You never ever can or should use a dimension to change the hole size.

 

A Hole Feature as a so called super feature has its own parameters and those only can be modified by select and define them via the hole options menu.

 

The only dimensions within a hole feature are placement dimensions or dimensions to help geometry (construction geometry)

 

Go to the hole options and select what You need.

 

20160216_1218.PNG

regards
Wolfgang