Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a KILL SWITCH in solid edge?

Valued Contributor
Valued Contributor

Hello Community!

Sometimes my solid edge takes a lot of time to process any changes made, so, I was wondering if there is any KILL SWITCH in solid edge. LIke to stop the current process or las command?

Regards,

2 REPLIES 2

Re: Is there a KILL SWITCH in solid edge?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I believe that the ESC key will stop some long running processes like drawing view updates or even loading of a large assembly.  Can't find the documentation on it at this time.



Ken
Production: SE 2019 MP8, Testing: SE 2020
http://Grundey.blogspot.com

Re: Is there a KILL SWITCH in solid edge?

Valued Contributor
Valued Contributor
Thank you Grundey!

I always smash esc keys whenever I find myself in such situations, but ther aren´t effective. Anyway thank you!