Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there a shortcut to collapse the pathfinder?

Valued Contributor
Valued Contributor

I know i can right click on the top of the path finder and collapse - but if the path finder is quite long its hassle to scroll all the way up. 

Regards,

MagRiz
(ST9 User Est 01.18)
4 REPLIES

Re: Is there a shortcut to collapse the pathfinder?

Gears Honored Contributor Gears Honored Contributor
Gears Honored Contributor

There's no event or CommandID associated with the Pathfinder collapsing, so a macro hence  a shortcut is not possible. There might be some other way who might wantto share.

 

Re: Is there a shortcut to collapse the pathfinder?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MagRiz, as @Tushar says, there is no easy way to do this, such as adding it to the QAT.....another way is to double click [any of] the stack header[s] to toggle between expand & collapse. The problem is, as you say, when the pathfinder is very long, the main stack header is part of the scrolling bundle.

 

The best way to combat this condition, would be to make use of pathfinder groups, such as seen in this video.

 

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge 2019 [MP4] Classic [x3 Seats - Cloud Enabled]
Windows 10 - Quadro P2000

Re: Is there a shortcut to collapse the pathfinder?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@MagRiz  Not sure what the root issue is that you desire to regularly collapse the Pathfinder tree, but if it is to make it easier to find a component that was selected in the graphics window in a long Pathfinder tree, there is a Solid Edge Options setting in Assy under the Assembly section called "Auto-scroll assembly pathfinder" that will always cause it to scroll and expand to the selected component.



Ken
Production: SE 2019 MP4, Testing: SE 2020
http://Grundey.blogspot.com

Re: Is there a shortcut to collapse the pathfinder?

Valued Contributor
Valued Contributor

@KennyG

to tidy up the screen to see more of the model.

Regards,

MagRiz
(ST9 User Est 01.18)