Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there an easy way to customize the quick access toolbar?

Valued Contributor
Valued Contributor

Is there an easy way to customize the quick access toolbar? I have been going into each enviroment within the quick access and customizing by adding and removing the same commands. is there a mass change for all enviroment so i only have to do it once. then go in and modify the few difference?

Nathan M. Gardner

https://www.etsy.com/people/NathanMGardner

Be sure to check out my work!!
Made in Maine Wood Carvings

2 REPLIES 2

Re: Is there an easy way to customize the quick access toolbar?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@ngardner wrote:

Is there an easy way to customize the quick access toolbar? I have been going into each enviroment within the quick access and customizing by adding and removing the same commands. is there a mass change for all enviroment so i only have to do it once. then go in and modify the few difference?


That would be awesome but, alas, no. AFAIK

Bruce Shand
SE2019 MP5 - Insight - Win10 - K4200

Re: Is there an easy way to customize the quick access toolbar?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @ngardner

 

 

amazingly there is an Copy/Paste function within zhe Customizing form of Solid Edge, but the Copy only works for one and the same environment.

This would be great if a multiple selection and a copy/pase would work for several document types there

 

 

 

regards
Wolfgang