Showing results for 
Search instead for 
Did you mean: 

Is there an easy way to subdivide a line?


I have an operation that i use very often. I need to take a line or a distance between 2 points and equally sub-divide it to find a pacing that works.


what i do now is insert points and them space then manually by dividing the line length, but it is vert time consuming.

is there a feature like autocad that can divide a line into a number of equally spaced points or segments?


thanks for your help


Re: Is there an easy way to subdivide a line?

not a single command.


but you can use retangular pattern with option "fit to rectangle"... this at least auto calculate your equally divided segments


 then use the split command...




Matt Johnson
Solid Edge Certified Professional (ST7 & ST8)
Solid Edge ST9 (SEEC) - Production
NX11 (Tc Integration) Pre-Production Testing
Teamcenter 10.1.6