Is there an existing parts bin will items such as propellers and other windmill parts premade?

Experimenter
Experimenter

What I am looking for is a database of pre-designed parts in file types that can be downloaded.

I see no point in reinventing the wheel so to speak; and my skillset with Solid Edge is new.

 

This would save an enormous amount of time on my project development. Thank you!

 

Mark Moghab

2 REPLIES

Re: Is there an existing parts bin will items such as propellers and other windmill parts premade?

Esteemed Contributor
Esteemed Contributor
Hi Mark,

Common items, such as fasteners and the like, are you typical standard parts that populate a parts library. Something like your wanting gets toward a pretty speciallised area....but you could try searching sources such as CADENAS part community, or GrabCAD...and the likes. Hopefully someone has such a model they're willing to share with you.
Make use of the Solid Edge help files & tutorials also, as these are both very thorough.
Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP2] Classic [x2 seats]
Windows 10 - Quadro P2000

There are several options...   The following is directly...

Esteemed Contributor
Esteemed Contributor

There are several options...

 

The following is directly from the Solid Edge desktop: http://solidedge.partcommunity.com/PARTcommunity/Portal/solidedge

 

There is also http://www.Grabcad.com for a variety of models that are way beyond just "off the shelf" components and most vendors who sell components also offer models.

 

They don't have to be just Solid Edge models either as you can import a variety of file formats including Solid Works...


Thanks,
Ken

Production: ST9 MP10
Testing: ST10 MP3