Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any tool to check the wall thickness of irregular Body in Solid edge ???

Creator
Creator

I want to check the wall thickness of the irregular Body ,i am using solid edge ST7

2 REPLIES

Re: Is there any tool to check the wall thickness of irregular Body in Solid edge ???

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi there,

 

Have you looked at using either "Live Section" or "Section" tools.....if you have not used either of these, type one into the "Command Finder" [at lower right side of the graphics window], and follow that up by looking at the help file topics.

Sean Cresswell
Design Manager Streetscape Ltd
Solid Edge ST10 [MP8] Classic [x3 seats]
Windows 10 - Quadro P2000
Testing: Solid Edge 2019

Re: Is there any tool to check the wall thickness of irregular Body in Solid edge ???

Gears Phenom Gears Phenom
Gears Phenom

There is no other way "only" what was suggested by @SeanCresswell (SE CAD jockey Smiley Happy )

 

Hmm, or you can you Minimal distance from Measure group...

 

BR,

Imics
http://solidedgest.wordpress.com/