Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any way to create an attribute from a dimension?

Experimenter
Experimenter

If I create a block that has attributes, is there any way to pass dimensional variables to the block so I can "scan" the drawing file attributes (like AutoCAD) with either a PLM system or third-party application  to determine the dimensional values?

 

The goal is to enter a number of dimensions for a part once on the drawing when developing the geometery, rather than once there and another time in a spreadsheet or database that will allow me to easily search for parts to re-use them in other designs.

 

Is there any other workaround besides using blocks/attributes to accomplish the same goal?  

 

Thanks

 

2 REPLIES

Re: Is there any way to create an attribute from a dimension?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Any Dimension placed creates a variable in the variable table.  Each variable can be exposed as a file property.  File properties can then be searched or passed to another appiclation.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Re: Is there any way to create an attribute from a dimension?

Experimenter
Experimenter

Thanks for reply.  I'm looking for trying to translate dimensions somehow into conventional attributes like those of a typical ACAD format DWG file.