Cancel
Showing results for 
Search instead for 
Did you mean: 

Is there any way to keep the dimension at the intersection point when fillet the corner?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Is there any way to keep the dimension in place at the intersection point when fillet the corner, like "Keep constrained corners" in Solidworks?


Vsharp3.jpg

8 REPLIES 8

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pornthep-DTA

 

 

 

besides the fact that I never would fillet within a sketch (always use 3D fillet) Solid Edge will automatically snap onto that virtual corner when using PMI dims in 3D.

 

 

regards
Wolfgang

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Hi, Wolfgang

Thanks for your suggestion.
Actually, I want to fillet a path curve for the sweep command, which cannot be done in 3D. Man Sad



@hawcad wrote:

Hi @Pornthep-DTA

 

 

 

besides the fact that I never would fillet within a sketch (always use 3D fillet) Solid Edge will automatically snap onto that virtual corner when using PMI dims in 3D.

 

 




Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Hi @Pornthep-DTA

 

 

OK, as You said there are situations where it is necessary to fillet within one sketch.

 

So then I would suggest to dim it to the intersection point either with using the I-button on keyboard (Intersection) or with hovering over both elements.

 

Problem here would be, that such dimension are not driving dimensions, so You cann't modify Your lines.

 

My advise or my method in such cases is, to draw a small circle, connect it to both lines (implicit intersection) and use this one for dimensioning.

It's not perfect but it works!

 

(view in My Videos)

 

 

 

PS.: change the circle to construction would be a good advise too!

 

regards
Wolfgang

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Phenom
Phenom

If I need a fillet in sketch (wich I try to avoid), I draw the extention lines and change them to "construction lines"

QS6E1Ol

...........................................................................................................
Solid Edge 2019 & AutoCAD 2020 user

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Phenom
Phenom

In the sketch you can place a point and constrain it onto each line.

Then you can dimension to the point.
Sketch profiles in the modelling environments do not allow dimensioning to an intersection.

HP Z420 16GB RAM
Quadro K4000
SE2019 MP5 on Windows 10 Pro 64.

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

@beachcomber
I do just like what you have told, lay points on the intersections and then dimension to the points.
But it took a few more steps. and for many corners profile, it's not just "few steps".

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Pornthep-DTA  This does not work so well if creating sketches for Ordered features, but if using them for Synch features it works great...

 

The Fillet command bar has an option to not trim the lines when it adds the fillet (Fillet - No Trim).  This keeps the dimensions to the sharp edge.  If using the sketch to create Synch features you will still get the correct region.

 

It would be awesome if SE would change the command to actually split the lines where the fillet connects and change the lines to the sharp edge to construction...  You ought to create a Change Request by logging an IR for that.



Ken
Production: SE 2019 MP5, Testing: SE 2020
http://Grundey.blogspot.com

Betreff: Is there any way to keep the dimension at the intersection point when fillet the corner?

Gears Phenom Gears Phenom
Gears Phenom

@Joris wrote:

If I need a fillet in sketch (wich I try to avoid), I draw the extention lines and change them to "construction lines"

QS6E1Ol

 


I do this exact thing quite often, mainly when I need a certain radius and a dim. to the tangent face of it, or often when reverse engineering a part with multiple radi.

-Craig